SH-Mobile Consortium


RENESAS SITE

English | Japanese
SH-Mobile LAB Home
About SH-Mobile LAB
Research Topics
Members
Idea Competition
Idea Competition
SH-Mobile Laboratory 2006  Final Round of Judging
 
   
Presentations
Following on from the work sessions conducted over past half year, the students provided their idea presentations which they had put together in their various ways.
In addition to the core members of the SH-Mobile Laboratory, four guest judges were also invited to participate in judging the ideas.
Guest judges
Mr. Katsuhiko Ogawa Vice President, Director, NTT Cyber Solutions Laboratories
Ms. Chika Sekine President, Udit Inc.
Mr. Etienne Barral Journalist
Ikuya Kawasaki Deputy General Manager, System Solution Business Unit 2, System Solution Business Group, Renesas Technology Corp.
Presentation by Kazunori Gumizawa
Information - Landscape Our Town
Department of Architecture, Chiba University Graduate School of Science and Technology
Tools that I can attach to my own body and commit to (participate in) the urban environment. In other words, a proposal for tools and applications that enhance how we walk about, see, and talk.
View movie
Presentation by Sho Matsuo
Remind of Days -Mobile Interface Using Dialog-
Department of Human Communications at the Graduate School of the University of Electro-Communications
Proposal for MIND (Mobile INterface using Dialog), a tool for creating a dialog between users and their mobile tools based on the experiences they share.
View movie
Presentation by Tetsuya Yamamoto
Conversation nation 2029: proximate networking
Department of Electrical and Electronics Engineering, Graduate School of Science and Technology, Kobe University
A proposal for mobile tools that make it easy to initiate communication with the people around you, and to interact with a wide range of different people.
View movie
Presentation by Keisuke Fukushima
Mobile Estate / SNS.plugin
Department of Architecture, Faculty of Engineering, the University of Tokyo
Proposal to supplement traditional real estate contracts with a "third place" (neither home nor office) home that can be selected dynamically using mobile technology. The presentation also looks at the new forms of community and work that will take place in such an environment.
View movie
(The university departments indicated above to which the students belong are as of 2007/2/24.)
Judging
The guest judges and core members retired to a separate room where they spent approximately one hour discussing the entries. On returning to the students, they spent nearly another hour discussing the results.
Mr. Tanaka The content of the entries has changed considerably since passing the first round of judging.
Mr. Ogawa I guess this is a result of the competition system where everyone came together for work sessions.
Mr. Watanabe In addition to the work sessions, the students also produced blogs together with the members. Through this process, the members have been able to observe the students' ideas crystallize.
Mr. Ogawa It is an interesting way of going about things.
Mr. Watanabe In this sense, rather than being objective judges, it seems that the members have become more like supervisors at university.
Mr. Tanaka Even so, it seems that only about 10% of what we said got through.
Mr. Ogawa Did you also use presentations like these for the first round of judging?
Mr. Watanabe No, the first round consisted of judging written entries only. We reviewed the submitted entries and scored these on-line.
Mr. Ogawa It is unusual that no women made it through to the second round. Women seem to have a particular strength in the field of mobile phones. I think they were quicker to adopt the technology.
Mr. Tanaka Perhaps they were put off by the choice of 2029 as the year.
Mr. Ogawa That's probably correct. Women don't place such an importance on the future and instead their strength lies in proposals that deal directly with what it is they want. The choice of year was a bit SF oriented.
Mr. Takahashi Still, the SF aspects of the entries seem to have disappeared.
Mr. Barral Nor were there any entries from overseas. The content of the entries seems very parochial. By parochial, I mean oriented towards Japan. There was nothing about automatic translation, for example.
Mr. Tanaka Yes, the entries may well be biased towards daily life, particularly daily life in Japan.
Mr. Watanabe Instead of using social problems as a starting point, the logic of the entrants seemed to be based on taking as a starting point the elimination of their own dissatisfactions, the things that they were not satisfied with, and then generalizing from there.
Ms. Sekine The entries appear very much to have been created from things that are close to the entrants' own lives. Its not so much that they have no social applicability, rather it is that, being so personally oriented, the entries do not seem to have taken a broader view to encompass people from different cultures or backgrounds. They present a very meager image.
Mr. Watanabe Yes, there was something frustrating about them.
Mr. Tanaka I had hoped to draw out that aspect of the students ideas, but I wasn't able to do it very successfully.
Mr. Ogawa This idea of a "third place", how do the students interpret this?
Mr. Maeda I think the common meaning is of a place that is part way between the conventional ideas of public and private.
Mr. Ogawa It can be thought of as a place that has become a part of the scenery, like a French cafe, Japanese izakaya or English pub, or simply as a halfway house.
Mr. Tanaka It seems that there are a growing number of young people whose idea of a third place is "somewhere where the normal conventions of human interaction are temporarily suspended" or "somewhere where you can interact with other people under the guise of a different personality".
Mr. Ogawa Perhaps you could call that a "fourth place".
Ms. Sekine That meaning is a little different to what is normally meant by "third place".
Mr. Maeda It is like the way those people in Harajuku who dress up in "Gothic and Lolita" clothing have brought a virtual layer to the physical world that is separate from ordinary day-to-day life. In the extreme sense of the term, it could be that a third place is thought of by young people as somewhere you can do this in a virtual world.
 
Final judging
The final round of judging involved the core members and guest judges being allocated points which they then awarded to the ideas they found most interesting.
Because the core members had been able to observe the ideas as they were fleshed out in the work sessions and blogs, they were only allocated with three points each.
The guest judges on the other hand were able to make a fresh evaluation of the entries based on the presentations and judging discussion and so were allocated six points each.
The points awarded to each entry were tallied and the winner of each prize selected.
 
Announcement of competition results
The judging took place after the completion of the presentations. The winners were selected and the prizes awarded as follows.
Top prize
Tetsuya Yamamoto
Excellence prize
Keisuke Fukushima
Kazunori Gumizawa
Encouragement prize Sho Matsuo
 

Back row, from left: Mr. Takahashi, Mr. Tanaka, Professor Nakajima, Mr. Watanabe, Mr. Maeda
Middle row, from left: Mr. Etienne Barral, Ms. Sekine, Mr. Ogawa, Mr. Kawasaki
Front row, from left: Mr. Matsuo, Mr. Fukushima, Mr. Yamamoto, Mr. Gumisawa


(C) 2003-2007 Renesas Technology Corp. All rights reserved.